Maintain Data Integrity

Some instructions and techniques can cause data loss or corruption. To maintain data integrity, follow these guidelines:
  • Use timers to control sequencing and prevent premature updates.
  • Apply scan-dependent logic so actions occur only once per scan for consistency.
  • Manage structured data with arrays and shift instructions, ensuring proper indexing and controlled movement to avoid overwriting values.
  • Perform SSV instruction changes only under stable conditions after data updates are complete.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal