Update the Redundancy Module Firmware in the Secondary Chassis

IMPORTANT: To maintain the crossload communication path between redundant modules during the update process, you must update the redundancy module firmware in the secondary chassis before the primary chassis. If you only have physical access to the primary chassis, then the secondary chassis must be updated first to ensure a valid communication path.
To update the redundancy module firmware in the secondary chassis, complete these steps.
  1. Launch
    ControlFLASH Plus®
    software.
  2. Update the redundancy module firmware.
  3. Close the
    ControlFLASH Plus®
    software.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal