MSG Instruction Behavior During Qualification and Switchover

During qualification of the redundant chassis pair, MSG instructions operate as follows:
  • The status message on the front of the redundancy module displays QFNG for qualifying.
  • If a configured message is cached, the primary controller automatically establishes a connection with the secondary controller with no errors.
  • If a configured message is uncached or unconnected, the message experiences the following error: Error 1 Extended Error 301, No Buffer Memory.
During a switchover, MSG instructions operate as follows:
  • In the primary controller, the message instruction status bits update asynchronously to the program scan. Consequently, you cannot crossload your message instructions status bits to a secondary controller.
  • Any active message instructions in the old primary controller become inactive. When the switchover occurs, you must reinitialize the execution of your message instructions in the new primary controller.
  • Cached and connected messages cause the message instruction to pause for 7.5 seconds because the primary controller has not received a response from the secondary controller:
    • For cached messages, the message instruction tries to execute three more times, each attempt followed by a pause of 7.5 seconds. If 30 seconds pass and the targeted controller does not respond to the initiating controller, then the switchover errors out with connected timeout Error 1 Extended Error 203. An example of a connected message is CIP™ data table read-and-write messages after a connection has been established.
    • Uncached messages error out after 30 seconds if you have initiated them because the initiating controller never received a reply to the forward-open request. The error is Error 1F Extended Error 204, an unconnected timeout. Examples of uncached messages include CIP generic messages and messages that are captured during the connection process.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal