Notification in the Tag Monitor
General module faults are also reported in the Tag Monitor. Diagnostic faults are reported only in the Tag Monitor. When the Value field is set to 1, a fault is present.
I/O Module Fault

Safety I/O Connection Fault

Provide Feedback