Distinguish between Standard and Safety Components

Components of a safety system that are not used by the safety function can be populated with other modules that are certified to the Low Voltage and EMC Directives. See the Rockwell Automation Product Certifications page () to determine that the modules have the CE certificate.
You must create and document a clear, logical, and visible distinction between the safety and standard portions of the controller project. As part of this distinction, the
Studio 5000 Logix Designer®
application features safety identification icons to identify the safety task, safety programs, safety routines, and safety components.
In addition, the Logix Designer application uses a safety class attribute that is visible whenever safety task, safety programs, safety routine, safety tag, or safety Add-On Instruction properties are displayed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal