Produce a Safety Tag

Complete these steps to produce a safety tag.
  1. In the project of the producing controller, create a user-defined data type that defines the structure of the data to be produced.
    Make sure that the first data member is of the CONNECTION_STATUS data type.
  2. Right-click Controller Tags and select New Tag.
  3. On the New Tag dialog box, set the type as Produced, the class as Safety, and the data type to the user-defined data type that you created.
    Produced Safety Tag
  4. Click Connection and enter the max limit on the number of consumers (1…15).
    Produced Tag Connection
  5. Click OK.
  6. Click Create.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal