Create Tag Mapping Pairs
- From the Logic menu, select Map Safety Tags.

- In the Standard Tag Name or Safety Tag Name column, enter or select an existing tag:
- To show only controller-scoped standard tags, click the arrow in the Standard Tag Name column.
- To show only controller-scoped safety tags, click the arrow in the Safety Tag Name column.

- In the Standard Tag Name or Safety Tag Name column, add a new tag:
- Right-click in the empty cell.
- Select New Tag.
- Enter the tag name into the field.
- Right-click the field and select New tagname, where tagname is the text you entered in the field.
Provide Feedback