Use AutoFlash to Update Firmware

To update your controller firmware with the AutoFlash feature, complete these steps.
IMPORTANT:
If the Secure Digital Card is locked and set to load on power-up, then this update can be overwritten by firmware on the SD card.
  1. Verify that the network connection is made and your network driver is configured in Linx-based communication software.
  2. On the Path bar in the programming software, click the Network Browser.
    This image shows how to access the Network Browser.
  3. On the Network Browser, select your controller under the communication driver you want to use, and click Update Firmware.
    This image shows a selected controller and the Update Firmware button.
  4. On the Choose Firmware Revision dialog box, browse to the location of the firmware files.
    This image shows how to select a firmware revision.
  5. Select the firmware revision and click Update.
  6. On the Confirmation dialog box, click Yes.
    This image shows Update Firmware confirmation dialog.
    The firmware update begins.
    Allow the firmware update to complete without interruption. When the firmware update is complete, the process dialog box closes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal