Online edits that require an SFC reset
These tables indicate which online edits require a reset and which online edits do not require a reset:
Step Element | Requires an SFC Reset |
Create a Step | Y |
Reposition a Step (without rewiring) | N |
Rewire a Step | Y |
Cut, Paste, or Delete a Step | Y |
Copy a Step | N |
Change the type of a Step (Initial or Normal) | Y |
Change the Expression used to calculate a Step Preset value | N |
Change the Preset, Timer, Timer Max, or Count value for a Step | N |
Change the Pause Timer When Routine is Paused configuration for a Step | N |
Change the Alarm Enable configuration for a Step | N |
Change the Expression used to calculate a Step Limit High, or Limit Low value | N |
Change the Limit High or Limit Low value for a Step | N |
Change the name of a Step to reference a different tag | Y |
Change the name of a Step to reference an alias for the tag | N |
Create or change a Step description | N |
Reposition a Step description box | N |
Hide or Show the description for a Step | N |
Change the Action execution order for a Step | Y |
Temporarily Hide or Show actions for a Step | N |
Persistently Hide or Show actions for a Step | N |
Transition Element | Requires an SFC Reset |
Create a Transition | Y |
Reposition a Transition (without rewiring) | N |
Rewire a Transition | Y |
Cut, Paste, or Delete a Transition | Y |
Copy a Transition | N |
Change a Transition Condition | N |
Change the name of a Transition to reference a different tag | Y |
Change the name of a Transition to reference an alias for the tag | N |
Create or change a Transition description | N |
Reposition a Transition description box | N |
Hide or Show the description for a Transition | N |
Action Element | Requires an SFC Reset |
Create an Action | Y |
Change the Action execution order for a Step | Y |
Cut, Paste, or Delete an Action | Y |
Copy an Action | N |
Change the type of an Action (Boolean or non-Boolean) | Y |
Change an Action Qualifier | Y |
Change the Expression used to calculate an Action Preset value | N |
Change the Preset, Timer, or Count value for an Action | N |
Change the Pause Timer When Routine is Paused configuration for an Action | N |
Change the Indicator Tag for an Action | N |
Change the Indicator Tag value | N |
Change an Action Body | N |
Change the name of an Action to reference a different tag | Y |
Change the name of an Action to reference an alias for the tag | N |
Create or change an Action description | N |
Temporarily Hide or Show actions for a Step | N |
Persistently Hide or Show actions for a Step | N |
Stop Element | Requires an SFC Reset |
Create a Stop | Y |
Reposition a Stop (without rewiring) | N |
Rewire a Stop | Y |
Cut, Paste, or Delete a Stop | Y |
Copy a Stop | N |
Change the name of a Stop to reference a different tag | Y |
Change the name of a Stop to reference an alias for the tag | N |
Create or change a Stop description | N |
Reposition a Stop description box | N |
Hide or Show the description for a Stop | N |
Simultaneous Branch | Requires an SFC Reset |
Diverge or converge wiring to form a Simultaneous Branch | Y |
Reposition a Simultaneous Branch (without rewiring) | N |
Rewire a Simultaneous Branch | Y |
Cut, Paste, or Delete a Simultaneous Branch | Y |
Copy a Simultaneous Branch | N |
Reposition a Simultaneous Branch leg (without changing the wiring) | N |
Add or remove Simultaneous Branch legs | Y |
Selection Branch | Requires an SFC Reset |
Diverge or converge wiring to form a Selection Branch | Y |
Reposition a Selection Branch (without rewiring) | N |
Rewire a Selection Branch | Y |
Cut, Paste, or Delete a Selection Branch | Y |
Copy a Selection Branch | N |
Reposition a Selection Branch leg (without changing the wiring) | N |
Add or remove Selection Branch legs | Y |
Change the Sequence Priorities for the Selection Branch leg evaluation order | Y |
Wire | Requires an SFC Reset |
Connect a wire to or disconnect a wire from an element or branch | Y |
Cut or Delete a wire | Y |
Hide or Show a wire | N |
Subroutine/Return Element | Requires an SFC Reset |
Create a Subroutine/Return element | N |
Reposition a Subroutine/Return element | N |
Cut, Paste, or Delete a Subroutine/Return element | N |
Copy a Subroutine/Return element | N |
Make changes to the lists of Input or Return parameters for a Subroutine/Return element | N |
Text Box Element | Requires an SFC Reset |
Create a Text Box | N |
Reposition or resize a Text Box | N |
Cut, Paste, or Delete a Text Box | N |
Copy a Text Box | N |
Attach a Text Box to or Detach a Text Box from another element | N |
Change the text within a Text Box | N |
SFC Forces | Requires an SFC Reset |
Change a Transition force | N |
Change a Simultaneous Branch leg force | N |
Enable or disable SFC forcing | N |
Provide Feedback