Replace dialog box parameters
Use the
Replace
dialog box to specify what to replace and where to search. The dialog box contains the following parameters.Parameter | Description |
Find What | Specify what to search for. Enter a new string or select a previously-searched string from the pull-down list. When the Find dialog box opens, this field contains either the selected text, or the text on which the caret is located.The list of previously-searched stings is the same list that appears in the History list on the standard toolbar. Searched-for items are added to the top of the previously-searched string list.Tip: To search for an instruction, type the instruction's mnemonic (for example, ADD). To search for a rung edit zone, enter the ^ character (for example, ^r indicates a search for a pending edit replace).Click the ... button ( ), located to the right of the Find What field, to display the Search Item Browser dialog, and choose an item to search for. The ... button is only enabled when Limit To is set to Text Only , References to Exact Tag and Its Members , or References to Tag . |
Limit To | Choose an option from this menu to configure what the Find What field represents.Tip: This option is not available when searching within the Tag Editor/Data Monitor. |
Replace With | Specify what to replace the Find What string with. Enter a new string or choose a previously-used string from the pull-down list.To specify an instruction, type the instruction’s mnemonic. Tip: Cannot replace logic, tags or comments while online. It is possible to rename a program while online.Click the button located to the right of the Replace With field to display the Search Item Browser dialog, and choose an item to use as a replacement. |
Find Where | Select the range in which the search will be performed. When the scope to search spans multiple routines or tag listings, the order in which components are searched is the order in which they are displayed in the active organizer. The available options depend on which searchable window is active. |
Wrap | Select this option to wrap the search back to the beginning, once the end of the current scope is reached. When enabled, Find automatically wraps to the beginning. This option is selected by default. |
Match Whole Word Only | Select this option to instruct the search to only find complete words. This includes underscore characters, all punctuation marks, and any printable character that is not valid in a tag name. This option is always selected with Use Wildcards . |
Use Wildcards | Select this option to enable the use of wildcard characters in the Find What and Replace With fields. When selected, use an asterisk ("*") to substitute for zero or more characters. This function is available only when Find Where is set to All Programs , All Programs in Current Task , or All Programs in Current Program .Multiple wildcard characters are permitted, but consecutive wildcard characters ("**") are not permitted in the Find What field. They are allowed in the Replace With field.In the Replace With field, a wildcard character substitutes for any text matching the corresponding wildcard character in the Find What field as part of the find operation. The Replace With field must contain the same number or fewer wildcard characters than the Find What field. If the Replace With field contains fewer wildcard characters than the Find What field, the text matching the last unmatched wildcards is discarded. |
Direction | Select Up or Down to specify the direction to search, relative to the current position within the active searchable window.The direction of the search can extend across multiple routines or tag collections; the search order mirrors the order of the items in the active organizer. The default direction is Down . |
Find Within | This area indicates where the Logix Designer application will search. Commas separate each search location. Click Find Within to expand this section of the dialog box and display options specific to each type of search component. |
Find Next | Click this button to activate the search. |
Find All | Click this button to find every occurrence of the specified string in the Find What field. The results of the search are written to the Search Results tab of the Output window. Click a search result to navigate to that location. |
Replace | Click this button to find the first occurrence of the string specified in the Find What field. If nothing is found to replace, a message appears to indicate that nothing was found.Clicking this button when an occurrence of the specified string is selected replaces the selected item with the string in the Replace With field. |
Replace All | Click this button to replace every occurrence of the Find What string with the Replace With string.The results of the Replace All action are written to the Search Results tab of the Output window. |
Provide Feedback
), located to the right of the
button located to the right of the