PMTR HMI command buttons
Use the
Command configuration
tab on the PMTR Properties
dialog box to label the HMI command buttons for Process Motor (PMTR) instructions.To label HMI command buttons for PMTR instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
. - In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Under theHMItab, selectCommand configuration.
- For each HMI command, enter these labels. The labels appear on the HMI.
- In theCommand buttonbox, enter the label for the command, such as Start slow, Stop, or Jog forward.
- In theTarget statebox, enter the text that appears for the target state; for example, Running slow, Stopped, or Jogging forward.
- In theTransition statebox, enter the text that appears during the transition state; for example, Starting slow or Stopping.
- When online with the controller, monitor theDevice stateandDevice issuesindicators at the bottom left of the dialog box:
- Device state. Displays the current device state, such asRunning,Stopped, orOut of service.
- Device issues. Displays fault conditions, such asFail to startorConfiguration error.
- SelectApply.
Provide Feedback