HMI navigation for PINTLK
Use the
HMI > Navigation
tabs on the PINTLK Properties
dialog box to enable or disable navigation from the HMI to interlock objects.To enable HMI navigation to interlock objects for Process Interlocks (PINTLK) instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
. - In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Under theHMItab, selectNavigation 0-15orNavigation 16-31.
- To allow navigation to an interlock object from the HMI faceplate, selectAllow navigation.
- In theObject tag namebox, enter the path and tag name for navigation to the destination object.
- SelectApply.
Provide Feedback