Enable and disable device Automatic Diagnostics

Automatic Diagnostics automatically sends device diagnostic condition updates to applications and client devices supported by
FactoryTalk Alarms and Events
. Automatic Diagnostics is enabled by default on supported devices.
TIP:
Automatic Diagnostics is supported only on
CompactLogix
5380,
CompactLogix
5480,
ControlLogix
5580,
Compact GuardLogix
5380, and
GuardLogix
5580 controllers.
To Enable or disable Automatic Diagnostics for a device:
  1. In the
    I/O Configuration
    tree, right-click a device and select
    Properties
    to open the
    Module Properties
    dialog box.
  2. Select the
    Connection
    tab.
  3. Select or clear the
    Enable Automatic Diagnostics
    check box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal