Logical Organizer icons
The
Logical Organizer
window is a graphical representation of the logical organization of your project that you can resize, undock, dock, and move. It contains a hierarchical tree of the programs and folders that contain information about the programs in the current project. The following tables describe the icons that can appear in the Logical Organizer
.Icon | Description | Icon | Description |
Open folder | Function block routine | ||
Closed folder | Sequential function chart routine | ||
Tags folder | Structured text routine | ||
Program | Equipment Phase | ||
Ladder routine | Equipment Sequence | ||
Main ladder routine | Ladder phase state routine | ||
Main safety ladder routine | Function block phase state routine | ||
Locked routine | Sequential function chart phase state routine | ||
![]() | Folder that cannot participate in the execution model (open) | Structured text phase state routine | |
![]() | Folder that cannot participate in the execution model (closed) | ||
![]() | Safety folder that cannot participate in the execution model (open) | ||
![]() | Safety folder that cannot participate in the execution model (closed) |
Provide Feedback