Failed to modify the properties for the routine <Routine Name>

Tried to change a property of a routine within the Routine Properties dialog box, but the operation did not succeed. This could be because:
  • the given name was invalid
  • the routine was deleted
  • the program the routine is contained in was deleted
  • there is insufficient memory
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal