Actions impacting components when a permission set is applied
When you apply a permission set to a tag, routine, or Add-On Instruction definition, several actions are involved in controlling a user's ability to view, change, or delete that project component. The following table lists the actions that apply to different types of components.
FactoryTalk Administration Console Action | Routines | AOIs | Tags | Effect |
Add-On lnstruction: Delete | ![]() | Controls ability to delete an AOI. | ||
Add-On lnstruction: Export | ![]() | Controls ability to export an AOI. | ||
Add-On lnstruction: Export Unencoded | ![]() | Controls ability to export an AOI in clear text. | ||
Add-On lnstruction: Modify | ![]() | Controls ability to modify an AOI. | ||
Add-On Instruction: View Logic | ![]() | Controls ability to view the internal information in an AOI. | ||
Component: Modify Permission Set | ![]() | ![]() | ![]() | Controls ability to modify a permission set associated with a component. |
Routine: Delete | ![]() | Controls ability to delete a routine. | ||
Routine: Export | ![]() | Controls ability to export a routine. | ||
Routine: Export Unencoded | ![]() | Controls ability to export a routine in clear text. | ||
Routine: Modify Logic | ![]() | Controls ability to modify the logic in a routine. | ||
Routine: Modify Properties | ![]() | Controls ability to modify the properties of a routine. | ||
Routine: View Logic | ![]() | Controls ability to view the logic in a routine. When permission to view logic is denied, permission to modify is also denied. | ||
Safety: Modify Component (applies only to the safety version of the component) | ![]() | ![]() | ![]() | Controls ability to modify a Safety component. Additional permissions might be required depending on the component. |
Tag: Delete | ![]() | Controls ability to delete a tag. | ||
Tag: Modify Constant Property | ![]() | Controls ability to designate a tag as constant. | ||
Tag: Modify Constant Tag Values | ![]() | Controls ability to modify the value of a constant tag. Also requires Tag: Modify Values . | ||
Tag: Modify Properties | ![]() | Controls ability to modify the properties of a tag, other than Constant designation. | ||
Tag: Modify Values | ![]() | Controls ability to modify the values of a tag. |
Provide Feedback