No support of embedded Ethernet port with redundancy
For the ControlLogix 5580 and GuardLogix 5580 controllers, redundancy does not support any use of the controller's Ethernet front port, including I/O, messaging, and downloading.
Select
Yes
to enable redundancy and remove support of the embedded Ethernet port. Select No
to maintain support of the embedded Ethernet port and remove redundancy. Provide Feedback