Failed to change the online EtherNet/IP Mode

Problem
Changing the
EtherNet/IP Mode
is not allowed because the connection to the controller via the specified port would result in loss of communication. This may occur under the following conditions:
  • Changing from A1/A2: Dual-IP mode to A1/A2: Linear/DLR mode and the connection to the controller is via the A1 port.
  • Changing from A1/A2: Linear/DLR mode to A1/A2: Dual-IP mode and the connection to the controller via the A1/A2 port does not have an Ethernet cable connected to the physical A2 port.
Solution
To change the
EtherNet/IP Mode
, select a different communication path.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal