Failed to launch RSLogix Fieldbus Manager

RSLogix Fieldbus Manager could not be launched.
An error occurred when either locating the RSLogix Fieldbus Manager program file or executing it. Refer to the message box for the exact cause of the error.
If this problem continues, launch RSLogix Fieldbus Manager manually using the Start > Programs option.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal