Controller Properties dialog box - General tab

Use the settings on the
General
tab to view or change the controller name and description, as well as the physical properties of the controller.
TIP: To open the Controller Properties dialog box - General tab:
  1. On the
    Online
    toolbar, click the
    Controller Properties
    icon.
  2. On the
    Controller Properties
    dialog box, click the
    General
    tab.
Use the
General
tab to:
  • View the type and revision of the controller.
  • View the vendor of the controller.
  • Enter or change the name of the controller.
  • Enter a description for the controller.
  • If applicable, enter a slot or chassis type for the controller.
  • Change to a different controller type or revision.
  • Change the EtherNet/IP mode of Ethernet ports if the controller supports one or more configurable Ethernet port pairs, for example,
    CompactLogix
    5380.
On controllers protected with
FactoryTalk Security
, users must be granted the
Controller: Modify Properties
permission to edit controller properties.
TIP:
This tab can also appear in the
Connected
dialog box, so that you can view information from the attached controller without first having to correlate.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal