Importing an Add-On Instruction Definition

Perform this procedure when you want to use the definition for an Add-On Instruction that was exported from another
Logix Designer
application project. Once the project has the definition, you can use the instruction in your programs.
Does the
Logix Designer
application project already have a revision of this Add-On Instruction?
To import an Add-On Instruction definition
  1. In the Controller Organizer, right-click
    Add-On Instructions
    and choose
    Import Add-On Instruction
    .
  2. Find the file that contains the instruction definition that you wish to import.
  3. Select the file and choose
    Import
    .
  4. Click
    OK
    .
The definition has been added to your project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal