Adding to the Signature History
The Signature History on the Signature tab of the Add-On Instruction Definition dialog box is an extension of the current Change History. Entries include the user name, Signature ID, Signature Timestamp, and a user-definable description of the signature history entry.

- Up to 6 history entries are maintained with the most recent entry on top.
- You can copy single cells, individual rows or the entire grid contents to the clipboard in TSV (Unicode tab separated value) format to facilitate electronic documentation.
- The Last Edit Date/Time is modified by the creation of a history entry.
- The updated Last Edit Date/Time becomes the Signature Timestamp of the new entry.
To create a Signature History Entry:
- Select theAdd to Historybutton. TheCreate History Entrydialog box opens.TIP:The Add to History button is only enabled when the Add-On Instruction is offline and sealed.
- Enter a description of the signature entry. Note the following:
- The description can be up to 513 Unicode characters.
- The description is not translatable once the Add-On Instruction is sealed.
- SelectOKto create the entry. TheLast Edit Dateis modified and the new entry is added to the top of theSignature Historylist with the other entries (if present) moving down and the 6th entry discarded (the oldest entry).IMPORTANT:This is an immediate action that cannot be undone.
- SelectCancelto leave theSignature HistoryandLast Edit Dateunmodified.
Provide Feedback