Module-defined Data Types (CONTROLNET-MODULE)
The table below lists and describes module-defined data types for the CONTROLNET-MODULE module. The data types are listed below the way they are listed in the Controller Tags window from the
Logix Designer
Data Monitor. These tables include information for input (as indicated by an "I"), output (as indicated by an "O"), configuration (as indicated by a "C"), and status (as indicated by a "S").Module-defined Data Type: AB:CONTROLNET_MODULE_SINT_125Bytes:I:0
Name | Data Type | Default Display Style | Definition |
Data | Varies with Comm Format and size of Connection Parameters choices | Decimal | Vendor defined based on module selected. |
Module-defined Data Type: AB: CONTROLNET_MODULE_SINT_124Bytes:O:0
Name | Data Type | Default Display Style | Definition |
Data | Varies with Comm Format and size of Connection Parameters choices | Decimal | Vendor defined based on module selected. |
Module-defined Data Type: AB: CONTROLNET_MODULE:C:0
Name | Data Type | Default Display Style | Definition |
Data | SINT[400] | Decimal | The configuration data sent when opening the I/O Connection. While this member is of a fixed size (400 bytes), the amount of data sent for a particular module is determined by the Configuration Size connection parameter you specify on the CONTROLNET-MODULE General tab on the Module Properties dialog box. Size ranges from 0 to 400 bytes. |
Module-defined Data Type: AB: CONTROLNET_MODULE_SINT_500Bytes:S:0
Name | Data Type | Default Display Style | Definition |
Data | Varies with Comm Format and size of Connection Parameters choices | Decimal | Vendor defined based on module selected. |
Provide Feedback