Change the data table monitor file display properties

  1. From the data table display, select a data element.
  2. Right-click and select
    Properties
    .
  3. Enter the poll rate, between 250 and 34560000 milliseconds, that you wish the data table monitor to poll the processor for data. Due to current limitations, a valid data table monitor poll rate set to greater than 1000 ms will decrease the update rate of the data table display, but the processor will continue to be polled at 1000 ms.
  4. Click
    OK
    to return to the data table display. The property changes you made are reflected in the data table display.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal