Import or export alarms

Use
Alarm Import Export Wizard
to import or export alarms in
FactoryTalk View Studio
.Use
Alarm Import Tool
to import alarms without starting
FactoryTalk View Studio
.
You can export alarms, alarm messages, or both from one Tag Alarm and Event Server and then import them into another. This allows you to:
  • Move or copy alarms from one Tag Alarm and Event Server to another.
  • Use conversion programs to convert alarms from one alarms and events system to another.
  • Create alarms using programming tools such as
    Microsoft
    Visual Basic or C++ and then import an output file from the program.
  • Create alarms by adding alarms to an exported alarm file, for example, using Notepad.
  • Modify alarms by searching and replacing, for example, to replace one set of tags with another.
  • Translate alarm messages into other languages.
  • Generate reports about alarm definitions.
To export alarms from a Tag Alarm and Event Server, you must have
Common
>
Read
permissions for the server.
To import alarms into a Tag Alarm and Event Server, you must have the following security permissions for the server:
  • Common
    >
    Read
  • Common
    >
    Write
  • Alarming
    >
    Enable/Disable
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal