Security permissions for the Alarm Status Explorer

You can select only areas for which you have security permissions. Access to alarm sources is controlled by FactoryTalk Security:
  • If the user is denied
    Common > List Children
    access to an area, child areas are not displayed in the tree view, and alarms in the area are not displayed.
  • If the user is denied
    Common > Read
    access to an area, the area are not displayed in the tree view at all. Alarms within the area are also not displayed.
  • To enable or disable an alarm, you must have
    Alarming > Enable/Disable
    permission for the area containing the alarm.
  • To suppress or unsuppress an alarm, you must have
    Alarming > Suppress
    permission for the area containing the alarm.
  • To shelve or unshelve an alarm, you must have
    Alarming
    >
    Shelve
    permission for the area containing the alarm.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal