Elements on the Alarm Status Explorer
The
Alarm Status Explorer
is divided into two panes. The left pane contains the area tree and the right pane contains the toolbar, alarm source list, status bar and the alarm source filter.Interface element | Description |
|---|---|
Toolbar | The toolbar is displayed at the top of the Alarm Status Explorer . It contains these buttons: Enable the selected alarm. Disable the selected alarm. Unsuppress the selected alarm. Suppress the selected alarm. Unshelve the selected alarm. Shelve the selected alarm. Show details for the selected alarm. Refresh the information in the alarm source list. Open the Alarm Status Explorer Help. |
Area Tree | The area tree shows the FactoryTalk Directory area model and application. The first node displayed in the area tree (the root area) defaults to the application but can be changed. |
Alarm Source List | The right pane of the Alarm Status Explorer displays a list of alarm sources contained in the selected area and any areas below. The list is divided into columns that display information about a given alarm. Uses of the Alarm Source List:
|
Alarm Source List Status Bar | The Alarm Status Explorer status bar displays:
|
Alarm Source Filter | The contents of the alarm source list can be filtered by the alarm name or by the alarm status. Wildcard characters can be used to match one or more characters in an alarm name. |
Provide Feedback
Enable the selected alarm.
Disable the selected alarm.
Unsuppress the selected alarm.
Suppress the selected alarm.
Unshelve the selected alarm.
Shelve the selected alarm.
Show details for the selected alarm.
Refresh the information in the alarm source list.
Open the