Columns in the Alarm Status Explorer

The data in the
Alarm Status Explorer
alarm source list is organized into columns and represent the following alarm information.
Column
Description
State
Displays one of the following icons indicating the alarm state:
  • No icon—all of the alarm conditions for the alarm are Normal.
  • InAlarm One or more of the alarm conditions for the alarm are In Alarm.
  • Disabled The alarm is disabled.
  • UnknownState The state of the alarm is not known. This is typically displayed when the
    Alarm Status Explorer
    is starting up and is in the process of gathering alarm states.
  • InAlarmFaulted One or more of the alarm conditions for the alarm are In Alarm and faulted.
  • NotInAlarmFaulted One or more of the alarm conditions for the alarm are faulted.
Suppressed
If an alarm is suppressed, the Suppressed icon is displayed in this column.
Shelved
If an alarm is shelved, the Toolbar_Shelve icon is displayed in this column.
Alarm Name
The name of the alarm. For example, Tank1Level.
Path
The FactoryTalk Directory path to the area containing the alarm source, which optionally may include the alarm server associated with the alarm source, in the format:
/Application/Area1/SubArea1/:ServerName.
For example: /Brewing/Line1/MixingTank:RSLinx1.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal