Product updates and patches
FactoryTalk
Updater installs with Rockwell Automation
software products. Use the updater to get notifications about new Rockwell Automation
software versions and patches.FactoryTalk Updater
To send notifications about new versions and patches,
FactoryTalk
Updater requires access to the Download Center web service. Verify that the firewall does not block access to this URL: https://api.rockwellautomation.com/es-be-pcdc-vpcprod/. Registering for updates is not required to receive notifications from the FactoryTalk
Updater.System logs and some application data are stored in this folder:
C:\Users\Public\Documents\Rockwell\Updater\Data
The logs and application data can be helpful when contacting
Rockwell Automation
Technical Support. System logs are automatically deleted after 90 days.Product Compatibility and Download Center
Product Compatibility and Download Center enables you to download software updates, firmware updates, and patches.
Information | Answer ID | Link |
|---|---|---|
Changes to communications software | 1071412 |
TIP:
To be notified when new Product Updates or Patches are released, select the
Add to My Favorites
link at the bottom of the Knowledgebase Answer.Provide Feedback