Configure a FactoryTalk Linx Gateway

Configure a
FactoryTalk® Linx™ Gateway
by adding the device to the policy model, setting authentication credentials, and defining connection endpoints.
IMPORTANT: You can only deploy policy models to configured
FactoryTalk Linx Gateway
devices.
Install and configure the
FactoryTalk Linx Gateway
server as follows:
  • In
    OPC UA Server
    , select
    Enable certificate management by FactoryTalk Policy Manager
    .
  • In
    OPC UA Server
    EndPoints
    FactoryTalkLinxGatewayName
    , under
    Authentication Settings
    , select
    FactoryTalk Security User
    .
For more information, see FactoryTalk Linx Gateway Getting Results Guide, publication FTLG-GR001H-EN.
  1. To configure a FactoryTalk Linx Gateway
  2. In
    FactoryTalk Policy Manager
    , add the
    FactoryTalk Linx Gateway
    device to the policy model.
    For more information, see Add a device.
  3. To authenticate with username and password, in device
    PROPERTIES
    , set
    Username
    and
    Password
    .
    TIP: The
    Anonymous
    user is selected for authentication by default.
  4. Set connection endpoints.
To deploy the policy model to the configured
FactoryTalk Linx Gateway
, see Deploy a policy model.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal