Publish the object
Add an OPC UA server and publish the object that exposes an OPC UA
method.
- InProject view, right-clickOPC-UAand select .OPCUAServerappears underOPC-UA.
- InProperties, next toNodes to publish, select.
A configuration of nodes to be published appears underNodes to publish. - UnderConfiguration1, next toNodes, select.

- FromProject view, dragMyObject1next toNode1inProperties.
- (optional) Adjust other OPC UA server preferences. See Add an OPC UA server.
Provide Feedback