Password policy

BrowseName
PasswordPolicy
SuperType
Object(BaseObjectType)

Properties

Name
BrowseName
DataType
Description
Maximum password age
MaximumPasswordAge
The number of days that a password can be used before the user must change it.
Enforce password history
EnforcePasswordHistory
The number of unique new passwords that must be associated with a user account before an old password can be reused.
Minimum password age
MinimumPasswordAge
The number of days that a password must be used before the user can change it.
Minimum password length
MinimumPasswordLength
The fewest number of characters that can make up a password for a user account.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.