Add a login form (type)
Add a widget type from the template libraries.
- Add a preconfigured widget (type):
- In the toolbar, selectTemplate Libraries
- InLibraries, search forLogin form.
- UnderComponents, dragLogin formontoUIinProject view.
- InProject view, right-clickMainWindow (type)and select .
- InProperties, create a dynamic link betweenUsersand .
Provide Feedback