Apply a template

Place a template in a node in
Project
view
so that objects in the node use the template. If the template is a graphic element, drag the graphic element from the library into the editor.
  • From the main toolbar, select
    Template
    Libraries
    and then either:
    • Drag a template from the library into a node in
      Project
      view
      .
    • Drag a template that is a graphic element from
      Libraries
      into the editor.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.