Configure the Output panel
Output
panelChange the amount of information provided in the
Output
panel.By default, the
FactoryTalk Optix Studio
Output
panel shows these message types:= Error of maximum severity
= Warning of minimum severity
= Information notices
If you configure the
FactoryTalk Optix Studio
Options and enable Advanced mode
, these items are added to the Output
panel display:Verbose1
Verbose2
You can change the level of information displayed in the
Output
panel for all of your FactoryTalk Optix Studio
Platform modules or you can specify the information level for specific modules.To configure the information level to display
- In the main toolbar, selectOptions
.
- InFactoryTalk Optix Studio options, selectAdvanced mode, and then selectClose.
- CloseFactoryTalk Optix Studioand then reopen it for the updated options settings to take effect.
- Select the down arrow onOptions
to display the contextual menu, and then select
Module log level configurationto openModule log level configuration.NOTE: TheModule log level configurationdialog box contains a list of every module within the project. You can scroll up and down the list. - Set the information level:
- InDefault level, select the default maximum information level for messages generated by all modules.
- If useful, for each individual module, override the default level with a specific information level for that module.
- SelectClose
Provide Feedback