Value axis
Y axis of the values of a Trend Graph.
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Automatic scaling | AutoScale | Enable/disable resizing of the Y axis based on the minimum and maximum values displayed in the graphic at runtime. | |
Provide Feedback