Colorization mode

Set the colorization mode which will be used when applying the selected color to the image.
BrowseName
ColorizationModeEnum

Values

Value
DisplayName
Description
0
Replace
For each color found in the image replace it with the selected color.
1
Hue
Replace the original color hue with the selected color hue
2
Multiply
For each color found in the image multiply it with the selected color. If the selected color is black the resulting color will be black, if the selected color is white the resulting color will be the original.
3
Add
For each color found in the image sum it to the selected color.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.