Set Network Path in IntelliCENTER explorer

Use the
Set Network Path
tab to set, modify, or clear the network path.
  1. On the explorer bar, select Devices Icon
    Devices
    .
  2. Select
    IntelliCENTER
    .
  3. In the
    IntelliCENTER
    explorer, right-click the lineup and select
    Set Network Path
    .
  4. In
    Set Network Path
    , select a network and either paste the network path or
    Browse
    to a path.
    TIP: To clear a network path, select
    Delete
    .
  5. To start monitoring for the lineup, select
    Start Status Monitoring
    .
    TIP: To start status monitoring, set all network paths. If you do not want to start status monitoring, select
    Save and Close
    to save the network paths and continue working.
    TIP: To communicate with the controller, Add a VPN driver.
The
Set Network Path
tab becomes
Edit Network Path
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal