Set Network Path in IntelliCENTER Dashboard

Use the
Set Network Path
tab to set, modify, or clear the network path.
  1. On the explorer bar, select Devices Icon
    Devices
    .
  2. Select the
    IntelliCENTER
    tab.
  3. At the bottom of the
    IntelliCENTER
    explorer, select
    IntelliCENTER Dashboard
    .
  4. In
    IntelliCENTER Dashboard
    , right-click a lineup and select
    Set Network Path
    .
  5. In
    Set Network Path
    , select a network and then either paste or browse to the the network path.
    TIP: To clear a network path, select
    Delete
    .
  6. To start monitoring the lineup, select
    Start Status Monitoring
    .
    TIP: To start status monitoring, set all network paths. If you do not want to start status monitoring, select
    Save and Close
    to save the network paths and continue working.
    TIP: To communicate with the controller, Add a VPN driver.
The
Set Network Path
tab becomes
Edit Network Path
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal