Explorer bar
The explorer bar appears in the Explorer pane of the open project. Use the icons on the explorer bar to open the various explorers:
Item | Description |
|---|---|
System | Opens the System explorer.Use the System explorer to create FactoryTalk Smart Objects
and the programs within the System Objects. |
Devices | Opens the Devices explorer.Use the Devices explorer to view and manage the hardware
used in the project. |
Execution | Opens the Execution explorer that contains the executable
logic of a project.Use the Execution explorer to create a controller
application and to view and change tasks, programs, and routines. |
AI Agent | Opens the AI Agent explorer.Use the AI Agent explorer to work with AI Agent workflows,
including Plan mode and Build mode. |
Library | Opens the Library explorer.Use the Library explorer to add new definitions of Add-On
Instructions, Smart Objects, Data Types, and user-defined libraries to the
project. |
Provide Feedback