FactoryTalk Remote Access

FactoryTalk Design Studio
integrates with
FactoryTalk Remote Access
to connect from the cloud to controllers.
FactoryTalk Remote Access
enables remote access and remote assistance to industrial equipment associated with Ethernet connections through the
Stratix®
4300 Remote Access Router, the
FactoryTalk Remote Access
Runtime, or through industrial PCs and other products, such as
FactoryTalk Optix
panels with the
FactoryTalk Remote Access
Runtime license included.
FactoryTalk Design Studio
accesses
FactoryTalk Remote Access
endpoints with a custom
FTDS
user, which is automatically created as part of the
FactoryTalk Remote Access
configuration. In this way,
FactoryTalk Design Studio
endpoint access can be managed separately from other applications, enabling secure communications for all managed systems.
For more information on the network architecture and security design of
FactoryTalk Remote Access
and how it communicates using endpoints, see System Architecture in the
FactoryTalk Remote Access
Online Help.
For more information on the network architecture and security design of
FactoryTalk Remote Access
and how it communicates using endpoints, see System Architecture help in the .
To configure
FactoryTalk® Remote Access™
:
For an online demonstration of how to set up a
FactoryTalk Design Studio
connection through
FactoryTalk Remote Access
, see FTDS Cloud to controller.
The following figure shows an example of a
FactoryTalk Design Studio
connection through
FactoryTalk Remote Access
:
FactoryTalk Design Studio Connection to Controller through FactoryTalk Remote Access
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal