Set the device path
Use
Deploy center
to set, change, or clear the device path that
specifies the target controller for the deploy operation.- On the top toolbar, select
to open
Deploy center.TIP: You can also selectDeploy centerat the bottom of theDevicesexplorer. - OnDeploy center, in thePathcolumn, select
,
and then select Set controller path. - InSet device path, expand the target FTRA_VPN endpoint, right-click the controller, and then selectConnect.TIP: If you are connecting to the FTRA_VPN endpoint for the first time or have added a device, you may need to reconnect to the FTRA_VPN endpoint to see the controller under the FTRA_VPN endpoint.
- Expand the FTRA_VPN endpoint, and then select the controller.
- SelectOK.TIP: You can manually edit the device path.
The selected communication path is saved as the current device
path.
Provide Feedback