Library explorer
Use the
Library
explorer to move FactoryTalk Smart Object
definitions from the System
explorer for reuse. Reusing FactoryTalk Smart Object
s improves the modeling for a system or plant. To edit, allocate, and deploy a FactoryTalk Smart Object
, create an instance of the Smart Object in the System
explorer. You can also create a FactoryTalk Smart Object definition, Add-On-Instruction, or User-Defined Data Type in the Library explorer. All reusable components of a logical system model should reside in the Library.
TIP:
In the
Library
explorer, you cannot delete elements that have instances that are used in the project.To open the
Library
explorer, on the explorer bar, select
Library
.Library explorer

Provide Feedback