FactoryTalk Design Studio Release Notes

August 2026
These release notes apply to
FactoryTalk® Design Studio
version 2.06.00.
FactoryTalk Design Studio
is a web-based design environment for industrial automation systems. It allows management, deployment, and monitoring of project content to
ControlLogix®
and
CompactLogix®
controllers, and to devices in the Motor Control Center (MCC) Lineup.
Use
FactoryTalk Design Studio
to create efficient systems that support multiple controllers, multiple collaborating engineers in a single project, and scalable reusable content.
The Rockwell Automation Product Compatibility and Download Center (PCDC) provides product-related downloads including firmware, release notes, associated software, drivers, tools, and utilities. For
FactoryTalk Design Studio
, the PCDC (http://compatibility.rockwellautomation.com/Pages/home.aspx) shows the available firmware to download by the controller using lifecycle recommendations, such as preferred, managed, or limited.
These release notes summarize the new features in this release and describe any enhancements to previously released features. They also provide information about the corrected and known anomalies in the software and supplemental application usage notes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal