Redeploy a project

Redeploy a project to deploy that project to a different controller. Change the controller path and add or change the comment about the redeployment.
  1. On
    Deployment history
    , select the project to redeploy, and then select
    Re-deploy
    .
  2. In
    Set device path and add comment
    , change the entries in these columns for each controller:
    • Path
      . Enter the new IP address of the controller.
    • Comment
      . Add or edit the comment for the redeployment of the controller.
  3. Select
    Re-deploy
    .
  4. In
    Deployment warning
    , select
    Yes
    .
    A progress bar indicates the status of the current build and deployment for the controller.
  5. In
    Choose a controller to go online with after deployment ends
    , select a controller, and then select
    OK
    .
    TIP: You can be online with only one controller at a time. If you are currently online with a controller and choose to go online with a different controller, you automatically go offline with the current controller and all monitoring tabs are closed.
The project redeploys to the updated controller path.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal