- Using the software
- Ladder Editor
- Add-On Instructions
- Instructions
- Instruction set
- Code Editor Domain Specific Language Syntax
Edit the logic for an instance of an Add-On Instruction
Open the logic of an instance of an Add-On Instruction to:
- View the instruction in context.
- See the data values of the Add-On Instruction instance.
- Identify instruction calls that have tags used for data.
Prerequisites
To edit the logic for an instance of an Add-On Instruction
- In the Explorer, selectSystem.
- InSystem, expand theFactoryTalk Smart Objectand program and then double-click the routine.
- In the routine, right-click the title bar of the Add-On Instruction instance and selectOpen instruction logic. The read-only logic for the instance of the Add-On Instruction opens.TIP:
- Open the logic for a different instance of the Add-On Instruction from the routine. In the upper-right corner of the tab for the routine, select the drop-down arrow and select the instance and path.
- Open the logic for the definition of the Add-On Instruction from the routine. In the upper-right corner of the tab for the routine, select the arrow, and then from the list and select the Add-On Instruction at the top of the list. No path appears for the definition. You can edit the logic for the definition of the Add-On Instruction.
Provide Feedback