Reuse a rules file

Upload a rules file from another project and ask the AI Agent to create a rules file for your project from it.
  1. Prepare the rules file for reuse.
    1. Sign in to the project containing the rules file for reuse.
    2. In the
      AI Agent
      explorer, expand
      Files
      AI Agent-generated
      , and then double-click the rules file to reuse.
      The rules file opens.
    3. On the rules file tab, select
      Download
      .
      The rules file is downloaded to your computer.
  2. Upload the rules file as a design asset in your project.
    1. Sign in to your project.
    2. In the
      AI Agent
      explorer, select
      AI Agent session
      .
    3. In
      AI Agent Session
      , select Upload files
      Upload files
      , browse to the rules file, and then select
      Upload
      .
  3. Prompt the AI Agent to create a rules file from the uploaded file.
    The AI Agent reads the uploaded file and creates a project-specific rules file based on its content.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal