COM-related exception errors

General COM-related system or program errors can occur for any number of reasons in processing the import or export request. A generic error handling displays the routine that encountered the error and the reason for the error as supplied by the originator (function) of the error.
If this occurs, an error message shows and the import or export does not occur. Examples include:
FTB_EE_XML_export_COM_Error
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal