Status bar

The status bar at the bottom of the Editor window usually displays a text message or state on the left side and the standard Caps Lock, Scroll Lock, and Num Lock states on the right side. In addition, to the immediate left of the Num Lock state, the status bar may display one or more icons representing the state and status of the Editor and/or its data. The following is a list of states that may be displayed in the status bar:
Status bar states
Icon
Item
Description
FTB_database_icon
Database
The Editor is accessing data.
FTB_error_icon
Error
An error occurred when editing data.
FTB_info_icon
Information
The currently selected data is predefined and not editable.
FTB_warning_icon
Warning
A message displays a warning.
FTB_critical_icon
Critical
A message displays critical error information.
FTBNE_arch_question
Question
A message displays a question.
FTB_search_icon
Searching
The Editor is searching for data.
FTB_secure_icon
Secured
The currently selected data is secured.
FTB_print_icon
Printing
A report is being printed or previewed.
FTB_processing_icon
Processing
The Editor is processing data.
FTB_wait_icon
Waiting
The Editor is busy.
FTB_verification_icon
Verification
Data is being verified.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal