Menu bar

The menu bar is similar to the standard menu bar found on most Windows applications. The menu bar contains the drop-down menus for
File
,
Edit
,
View
,
Tools
, and
Help
.
Menubar
This table describes the menu bar commands:
Menu bar commands
Item
Definition
File
Provides options for creating new objects, printing objects, and exiting the Editor.
Edit
Provides options for deleting selected items and viewing item properties. You use the
Properties
option for editing various items.
View
Allows you to show or hide the toolbar and status bar. You can also specify how data is viewed in the Detail pane and set user preferences for the Editor.
Tools
Allows you to configure system properties.
Help
Provides you with on-line help and information regarding the software and the system.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal